This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Full HD DLP4710 Chipset Evaluation Module

Other Parts Discussed in Thread: DLP4710

About Full HD DLP4710 Chipset Evaluation Module:

It's frame rate ?

Whether support External synchronous trigger or not ?

We need a projection module for 3D projection scanning ,frame rate ≥50HZ , white light brightness more than 50lm , supporting External synchronous trigger ,

Is the DLP4710 Chipset Evaluation Module able to ater for your particular needs?

  • Hello Wenjuan,

    Thank you for your interest in our DLP Technology.

    For a resolution of 1920x1080 we support up to 60 Hz. If you are planning to reduce the resolution we can support up to 120Hz.

    We have a camera trigger signal on TSTPT_4 which can be used as an external trigger.

    Please let me know if you have any further questions.

    Thanks,

    Nadine