Hi everyone,
I have two question about the photodiode placed in the reflectance head in front of the halogen lamp:
- which is the aim of such light sensor? It is used from the board in order to set the right configuration during the SCAN or is it used only as additional information?
-where i can found the part number of the photodiode?
Thanks for the availability.