This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pattern of bit-plane interleaving

Part Number: DLPC350

Hello,

I have a Acer k138ST which has been modified for a research application, I believe this model contains a DLPC350 and DLP4500DMD.

My understanding is that the pulse width modulation used to create grey scale from the bit planes uses an interleaved/shuffled pattern both between colors and the bit-planes themselves. For example, this shuffling results in the blue channel LED being active 4 times for every frame, each ~750usec long.

Unfortunately the bit-planes for a single color are also shuffled/interleaved, which is problematic because my intended application requires that 1) the blue LED be turned on for only 50-100usec of the normal 750usec window and 2) that some form of grey scale spatial structure be maintained (~4 bit is fine). The first requirement (modified LED timing) is working fine, but the second requirement that I know the actual pattern of interleaving which I can't find in the technical documentation and have failed to measure with a fast photodiode. Without knowing this timing diagram, I could be activating the LED entirely within the lowest precision bit resulting in an effectively binary image.

So a series of contingent questions - 1) Can you please confirm that the shuffling/interleaving pattern is static and not dynamic within one video mode. 2) If static, can you provide me the timing diagram of this interleaving? 3) If no timing diagram exists (hard to imagine), can you suggest a way to measure the timing of these bit planes on this type of commercial setup?

Thank you very much!

  • Hey Cameron,

    Thanks for using the DLP forums! Sorry for the confusion, it looks like this is not the DLPC350 controller (typically used for industrial applications). I moved this thread over to the DLP Video and Data forum. They will do some additional digging to get you an answer, so look for something early next week.

    Best,
    ~Danny W
  • Super. Thanks very much for your help Danny.

  • Hello Cameron,

    Thank you for your interest in our DLP Technology.

    You are correct the frame will be split in different color segments and will be arranged to achieve the best image quality. Depending on the firmware and the sequence which is being used the arrangement doesn't change after being selected. So as long as you are not changing the input frame rate or changing the look the sequence will not change.

    We leave it up to our customers to pick the look and sequence for their end-application. You can use a photo detector to measure the specific timing for each color on your projector.

    Best regards,

    Nadine

  • Thanks Nadine,

    It is useful to know that the arrangement is constant.

    One clarification - you wrote "changing the input frame rate or changing the look the sequence will not change." Does "the look" mean display settings such as the resolution/source of the input video signal, or are you referring to the actual content of the image such as the frames in a movie? Presumably the prior, but important to confirm since I will be making these measurements on images and not movies.

    Kind regards,
    Cameron
  • Hello Cameron,

    We have the possibility in our firmware to provide different looks which basically defines the color temperature.

    As long as you are keeping the input constant and keep the color temperature the same the system is using the same sequence.

    I hope this will help.

    Best regards,

    Nadine