Other Parts Discussed in Thread: DLPC350
Hello everybody
I got a LC4500 electronic kit from Keynote Photonics (this board is only the elctronic part, i.e. comprising only the DMD board and the driver board. It works also with DLPLC4500 GUI from TI) and I need to be answered about an issue: it has a mini-HDMI input port.
I am using TI GUI for Lightcrafter 4500 version 3.0.1
My goal is to create a pattern sequence for a spectrometer application, so I want to activate column by column of the DMD.
I go to the "creating sequence" tab and I upload 256 images that I will project onto the DMD (each image represents an activated column).
For create the sequence I have to go to "pattern sequence" tab (variable exposure), select video port (mini-HDMI), start from frame index=0 and add that image to the sequence pressing the button "add pattern to the sequence" and so on up to frame index=255?
After that has the pattern sequence been created?
Another question: How can I decide to activate only an image of the pattern sequence created and go to the next one pressing a button?
Thank's