Hey, I am using DMD to project a laser image. In the experiment, I found some diffraction problems:
(1) I used a 1064nm Infrared laser as the input for two DMDs (Discovery 1100 - visible window and Discovery 4000 - NIR window). I saw two sets of diffraction pattern in the output for both DMDs. These two diffraction patterns are the same but very close to each other. I read the material in your website but it doesn't mention anything about this diffraction patterns.
(2) I used a 6328A He-Ne laser for that Discovery 4000 again. At this experiment, I saw two patterns again. However, at this time, these two patterns is kind of far away to each other. The envolop of that weaker diffraction lies at (6,6) order of the stronger diffraction pattern.
I am guessing that these weird result may be caused by the window but then I can't explain the DMD4000 with infrared input. I am also thinking some DMD structure is wavelength sensitive?
Have you ever got this problem before? Any suggestion is appreciated.
Jinyang