This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with loading image at once



I am using DLP Discovery 4000 board and my operating system is Windows Vista SP2. When I am going to load image at once,  the program crashes. I tried "DLP Discovery 4000 Explorer" and also used the DDC4000l.ocx activex in both LabView and MATLAB. In all cases, I can load block by block; but when I am going to load whole image at the same time (LoadToDMD(17,1) or LoadToDMD(17,0)) the program crashes. 

  • Can you post your Explorer script? I can try to duplicate what you are seeing and help.

     

    Eric

  • Dear

    we have 2 problems the first that we cant detect the DMD when we connect the DLP discovery 4100 to the computer using the software "D4100 explorer" , in fact we detect only the card  but not the DMD ( "DMD: no DMD". 

    the second is that we are trying to use labview in order to load an image but  we have not a big idea how it works can you please send us the code ( programme) used with labview to load image?

    thank you very much