Hello sir
I want to clarify some doubts about the D400 board.
The d4000 board which I am using is DLP® Discovery 4000 .55” XGA Type X Starter Kit.
The FPGA is already loaded with a program to display the image which is being loaded and by resetting the mirrors it will be displayed on the DMD chip.So for some projecting applications i have to use a light source to project the image displayed on the DMD.is this conclusion is correct or not? If this judgment is correct then which all type of sources can be used for the application?
if I want to do another application I have to program the FPGA using Xilinx ISE ? How ?
whether any demos or videos are available for help on doing dlp applications?
Also I have been using the Explorer software for all working with the board.Can I do applicatons without using the Explorer software?
Please reply .