Hello, Mr/Ms
I’ve been working on a special projector program using DMD. My research group has already bought the DLP®Discovery 4000 Starter Kit. This project is kind of different from the usual visual projector system. It is required a single frame of image with a grayscale of 8 bits to be displayed within 300 microseconds (probably this constraint could be extended a little bit , but not too much). Well, we only care about the “on” state of the micromirror device because the receiver woks as a integrator of the luminous intensity. Could this system be synthesized?