Hello, we are using DMD with the laser to do beam shaping. I have some questions about the power efficiency.
(1) DMD is designed for visible light but our laser is infrared (1064nm). Based on the energy efficiency measurement, we found the result is only about 20%. Is it normal??
(2) I tried to find sources to explain this big loss and found some material for window transmission. Is the data from this transmission from input to output (2 passes through the windows and one bounce off the DMD)?
(3) Does diffraction cause a severe energy loss? Can you tell me about the fraction of energy in the main order?
Thanks!!