Hello,
I read from the 0.7" 2xLVDS XGA document that the maximum illumination is: 25 W/cm^2 for the wavelengths between 400nm - 800nm using a CW source.
It also has a rating of 0.68 mW/cm^2 for wavelengths below 400nm. Is this still true for the UV coated DMD?
Our wavelength of interest is 355nm.
Also, is the 2xLVDS (D4000) rated differently than the LVDS (D3000) for maximum CW illumination?
Thanks,
Jason