This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pico PWRONZ line



Hi,

I checked the Structured Light app note and the Programmers' Guide and found that line 14 of the 24 pin output on the projector is listed as PWRONZ.

The only thing both the documents say is that "PWRONZ is an on/off toggle input for projector. Performs same function as push button on projector."

Can you give more information on how this can be utilized?

Specifically, what do I need to do to:

1. Power ON the projector

2. Power OFF the projector

3. Power ON and hold to send it into the test pattern mode.

All this will be happening from an Arduino Mega board. What voltages and durations are required to trigger the functions above?

Our application requires the Pico to be mounted in a relatively inaccessible location and having a wire connect Power On/Off control is useful.

 

Warm Regards,

Abe