Hi,
a customer of mine is looking for DLP9000FLS DLP9000BFLS. What is the difference between the two part number?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
a customer of mine is looking for DLP9000FLS DLP9000BFLS. What is the difference between the two part number?
Thanks.
Hello Leo,
There is no mechanical or electrical difference between them, but there was a process improvement that enabled increasing the illumination power from 400 - 420 nm nm to 10 W/cm2 for the DLP9000BFLS.
The DLP9000FLS will shortly change status and will not recommended for new designs. For 420 - 700 nm applications it makes no difference which part is used.
Fizix