Part Number: DLPLIGHTCRAFTER
I am interested in using the DLP Lightcrafter to image patterned light onto a brain. My intention is to remove the light drive and incident the DMD chip with a laser (473nm 300mW) that has been expanded. The laser beam will once again be expanded before targeting the brain.
I understand that coherent light sources are subject to diffraction which can augment the actual image projected.
1) If the DMD chip is incident with a laser will diffraction cause the image patterned to be different then the intended pattern?
2) If so, what are some low cost methods around this issue?