Part Number: DLPLIGHTCRAFTER
Tool/software: Code Composer Studio
Hello E2E Community,
For some background, I am working on the DLP LightCrafter kit, which is actually a LC3000 version from Keynote Photonics without the light engine.
I intend to use LCr for structured illumination project and eventually will build my own GUI with hardware software integration with outher ongoing projects.
For that, I've installed QT Creator, CCS and DVSDK (under VirtualBox with Ubuntu 10.04 LTS 32-bit) following the recommendations in user guides and e2e suport team (thanks!).
Now, because it looks like I will be playing around a lot with the software and firmware of LCr, it's possible that at some moment, the LCr stops booting and responding overall.
To avoid bricking the system, ideally I'd love to have an option revert back to factory settings of LCr at any moment, but I don't how can I do that, if loose the communication with it, or it's not booting at all.
Then, in this thread (e2e.ti.com/.../221678), I saw that something similar related to DM365 booting is poossible:
"The solutions will be saved in either the NAND Flash or the SD card based on the DM365 SW (booting from NAND/SD)".
My question is, can I boot LCr from SD card with my versions of firmware, and whenever I need to run the factory version, I simply remove SD card and it will boot with the factory settings?
If that's not possible, what else would you recommend to have always a way to revert to factory firmware for all for all components of LCr kit?
Thanks,
Karl