This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC200: MEM_ODT(AH12) pin output buffer value

Guru 10570 points
Part Number: DLPC200


Hello,

I have seen IBIS model of DLPC200.
a) It seems that MEM_ODT(AH12) pin uses 50ohm output buffer. So I thinks actual ODT buffer value is 50ohm. Is my understanding right?

b) Do you have possibly to be changed this value (50 ohm) by firmware update?

Best regards, RY