1. On page 53 of the DLPC910 Datasheet (Section 10.1.3.2.1 LVDS Output Bus Skew) the recommended skew from one bus to another is 100-200ps. Have I understood correctly that this is the skew between the corresponding bus clocks? In other words, if, say, we use bus A clock as the reference, bus B clock should be skewed by 100-200 ps relative to bus A clock, bus C clock should be skewed by 100-200 ps relative to bus C clock (equivalent to 200-400ps relative to bus A), and finally bus D clock should be skewed by 100-200ps relative to bus C clock (300-600 ps relative to bus A)?
2. It is also stated that total skew should be kept below the maximum skew for the DMD. On page 17 of the DPL9000 Datasheet it is stated that the skew of channel B relative to channel A should be no more than 1040 ps, and the same for channel D relative to channel C. Does this mean that the skew between channels B and D, B and C, A and D, A and C is irrelevant?
3. On page 54 of the DLPC910 Datasheet in table 29, what exactly is meant by the "bus group trace length"?
4. Could you please clarify how Example 1 and Example 2 in the table relate to the skew requirements? In example 2, why is there no delay between bus A and bus B, and bus C and D even though a 100-200 ps is recommended?