This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP-ALC-LIGHTCRAFTER-SDK: Is the Qt strongly recommended as the development tool with the DLP-ALC-SDK?

Part Number: DLP-ALC-LIGHTCRAFTER-SDK
Other Parts Discussed in Thread: TIDA-00254

I have built the SDK follwing the dlpu042 manual, and TIDA-00254(3D scanning application). Because I was making my own application with Visual Studio 2015(vc 14) for a long time, I want to import the SDK into

my application. By googling I heard that vc compiler can not use .a files but only .lib files. So I tried building the SDK with Cmake and visual studio 2015 and failed with a lot of errors.

May I ask what version should I use to build the SDK to .lib files, if TI ever built the SDK using visual studio? Thank you.

  • Hi Hanul,

    Here at TI, we have not built the SDK with anything other than QT so I'm afraid we won't be able to offer any assistance on the use of Visual Studio. If you get it working and have the steps it took, I know it would be well received if you shared those with the community because there are several others looking to do the same thing.

    Thanks,
    Paul