This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00254: calibration camera and the projector,

Part Number: TIDA-00254


Hello, ask a question, in the projector's configuration file, the default trigger mode is an external trigger, before the problem is encountered, if the use of external trigger, in the calibration camera and the projector, the projector did not play the corresponding Light; how should i solve this problem? Seek answers. Thank you