Other Parts Discussed in Thread: AM5728
Hi all,
I want to run the 3D scanner on my board.
Actually i am using
Chip : AM5728
Sdk : ti-processor-sdk-linux-am57xx-evm-03.00.00.04
Board : custom board
Camera : Point Gray FL3-U3-13E4M-C
Projector : DLP 4500EVM
I refer to the http://www.ti.com/lit/ug/tiduc48a/tiduc48a.pdf documentation steps , and build arago-core-tisdk-image refer to http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK?keyMatch=build%20arago-core-tisdk-image&tisearch=Search-EN-Support
But there are a lot of errors in my build process.
These errors are as follows :
Run MACHINE=am57xx-evm bitbake arago-core-tisdk-image command
ERROR: binutils-crosssdk-x86_64-linaro-2.25-r2015.01 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
releases.linaro.org/.../binutils-linaro-2.25.0-2015.01-2.tar.xz:
2017-05-22 15:13:18 ERROR 404: NOT FOUND.
ERROR: binutils-crosssdk-x86_64-linaro-2.25-r2015.01 do_fetch: Function failed: Fetcher failure for URL: 'releases.linaro.org/.../binutils-linaro-2.25.0-2015.01-2.tar.xz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/lgp/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-crosssdk-x86_64/linaro-2.25-r2015.01/temp/log.do_fetch.21438
ERROR: Task 1414 (/home/lgp/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils-crosssdk_linaro-2.25.bb, do_fetch) failed with exit code '1'
complete information
lgp@lgp-OptiPlex-380:~/tisdk/build$ MACHINE=am57xx-evm bitbake arago-core-tisdk-image Loading cache: 100% |####################################| ETA: 00:00:00 Loaded 2838 entries from dependency cache. WARNING: No recipes available for: /home/lgp/tisdk/sources/meta-arago/meta-arago-distro/recipes-multimedia/libav/libav_9.16.bbappend /home/lgp/tisdk/sources/meta-processor-sdk/recipes-core/udev/udev_182.bbappend NOTE: Resolving any missing task queue dependencies Build Configuration: BB_VERSION = "1.30.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "Ubuntu-14.04" TARGET_SYS = "arm-linux-gnueabi" MACHINE = "am57xx-evm" DISTRO = "arago" DISTRO_VERSION = "2016.05" TUNE_FEATURES = "arm armv7ve vfp thumb neon callconvention-hard cortexa15" TARGET_FPU = "hard" meta-processor-sdk = "HEAD:1686d851985872f34ca3a2c30d4a0726a20a5c99" meta-arago-distro meta-arago-extras = "HEAD:36598b78a6d9fbe442f93111f64d3413c04418a8" meta-qt5 = "HEAD:d715f2c1d340fa38f8a9860acc73de5e14a38b75" meta-networking meta-ruby meta-python meta-oe = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a" meta-ti = "HEAD:1ae0cadb1200d0007a779958e852a48379d42c26" meta-linaro-toolchain = "HEAD:0f2a4dd08ab06768cc998fe3f7236e3942f4a2cc" meta = "HEAD:b0b91490e4ede61a302eb547da2cc65aa7da87ff" NOTE: Preparing RunQueue NOTE: Executing SetScene Tasks NOTE: Executing RunQueue Tasks WARNING: binutils-crosssdk-x86_64-linaro-2.25-r2015.01 do_fetch: Failed to fetch URL http://releases.linaro.org/15.01/components/toolchain/binutils-linaro/binutils-linaro-2.25.0-2015.01-2.tar.xz, attempting MIRRORS if available ERROR: binutils-crosssdk-x86_64-linaro-2.25-r2015.01 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output: http://releases.linaro.org/15.01/components/toolchain/binutils-linaro/binutils-linaro-2.25.0-2015.01-2.tar.xz: 2017-05-22 15:13:18 ERROR 404: NOT FOUND. ERROR: binutils-crosssdk-x86_64-linaro-2.25-r2015.01 do_fetch: Function failed: Fetcher failure for URL: 'http://releases.linaro.org/15.01/components/toolchain/binutils-linaro/binutils-linaro-2.25.0-2015.01-2.tar.xz'. Unable to fetch URL from any source. ERROR: Logfile of failure stored in: /home/lgp/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-crosssdk-x86_64/linaro-2.25-r2015.01/temp/log.do_fetch.21438 ERROR: Task 1414 (/home/lgp/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils-crosssdk_linaro-2.25.bb, do_fetch) failed with exit code '1' NOTE: Tasks Summary: Attempted 317 tasks of which 311 didn't need to be rerun and 1 failed. Waiting for 0 running tasks to finish: Summary: 1 task failed: /home/lgp/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils-crosssdk_linaro-2.25.bb, do_fetch Summary: There were 2 WARNING messages shown. Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
I tried to skip the above steps run MACHINE=am57xx-evm bitbake dlp-sdk command
Copy dlp-sdk_2.0.bb, dlp-sdk, camera-sdk to the corresponding location
lgp@lgp-OptiPlex-380:~/tisdk/build$ MACHINE=am57xx-evm bitbake dlp-sdk
Loading cache: 100% |###################################| ETA: 00:00:00
Loaded 2838 entries from dependency cache.
WARNING: No recipes available for:
/home/lgp/tisdk/sources/meta-arago/meta-arago-distro/recipes-multimedia/libav/libav_9.16.bbappend
/home/lgp/tisdk/sources/meta-processor-sdk/recipes-core/udev/udev_182.bbappend
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing PROVIDES 'flycapture' (but /home/lgp/tisdk/sources/meta-processor-sdk/recipes-ee/dlp-sdk/dlp-sdk_2.0.bb DEPENDS on or otherwise requires it)
ERROR: Required build target 'dlp-sdk' has no buildable providers.
Missing or unbuildable dependency chain was: ['dlp-sdk', 'flycapture']
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
My dlp-sdk and camera sdk are downloaded with reference to the version of the document, the operation is also based on the documentation steps.
I tried to install ipk on the board, there was an error :
Collected errors:
* satisfy_dependencies_for: Cannot satisfy the following dependencies for dlp-sdk:
* flycapture (>= 2.9.3.43) *
* opkg_install: Cannot install package dlp-sdk.
But I have copied the corresponding file
root@am57xx-evm:/usr/share/ti/dlp-sdk# ls /usr/lib/libflycapture
libflycapture-c.so libflycapturegui-c.so
libflycapture-c.so.2 libflycapturegui-c.so.2
libflycapture-c.so.2.9.3.43 libflycapturegui-c.so.2.9.3.43
libflycapture.so libflycapturegui.so
libflycapture.so.2 libflycapturegui.so.2
libflycapture.so.2.9.3.43 libflycapturegui.so.2.9.3.43
Can you help me analyze the cause?
Thanks.