Other Parts Discussed in Thread: DLPC900
I have a PRO6500 from Wintech which is based on the DLP LightCrafter EVM.
Recently by accident the power for the projector was shutted down in the middle of a transfer of the firmware (I know, it sounds bad). Consequently the DLP connected with USB was not recognized anymore by he GUI or the operating system (I'm using Win10).
However, we managed to upload the bootloader through JTAG following the instructions in the User Guide (Pages 50-51): first we tried deleting only the first sector according to the instructions without success, but then we deleted all the sectors and programmed the bootloader again. With the second procedure the DLP was recognized again by the GUI, except that the GUI is now extremely slow, many times unresponsive to any button (including changing the tab) and we cannot send any command.
When it was connected for the first time we tried to transfer the firmware hoping it would solve the issue but then we got the message "Error: Unable to enter to programming mode", so we tried any other command and not even the reset is responding, we got the message "Error: Unable to reset the board" (image below). After any of these messages the GUI gets unresponsive and we must close it or disconnect the usb cable to try again.
I wonder if there is another version of the bootloader that works better, or if you have any suggestion it would be highly apprecciated. Currently I'm using the version of the tools in this link: http://www.ti.com/tool/dlpc900ref-sw
Thanks a lot and I'm looking forward for your fast response.