This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPD4X00KIT: Project Video via DLPD4X00KIT

Genius 5355 points

Part Number: DLPD4X00KIT

Hi Support,

Customer is considering to use Discovery 4100 to project video.

Video will be transferred to 4100 through its expansion connector.

Do you have design example on it?

Thanks.

  • Hello Ikon,

    This kit is designed for low level control, but could be programmed in the APPS_FPGA to accept input on the EXP connector.

    We do not have any example code for the APPS_FPGA that will take a video stream and format and control the bit planes and illumination for video projection.

    What are their requirement?  Is it possible that the DLPLCR6500EVM or DLPLCR9000EVM could meet their requirements.  It already has video input.

    Fizix