This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000X: DLP LightCrafter9000 Evaluation Module/labview

Part Number: DLP9000X


Hi,

I want konw the if the product (DLP LightCrafter9000 Evaluation Module) can connect to the labview now?

Thank you.

  • Hello Peter,

    Somehow I missed your message. 

    There are not any vi's written to interface to Labview at this time.  It would require writing library calls in Labview to the API.

    You can use the the source code to show how the LightCrafter9000EVM is being connected to and initialized.  The source code should also have the *.h files needed to set up the prototypes in the Labview library calls.  Also refer to the API Programmer's Guide.

    You should be able to find the links to useful documents here:  

    http://www.ti.com/tool/dlplcr9000evm 

    http://www.ti.com/lit/pdf/dlpu018 

    I hope this helps.

    Fizix