Hi!
I'm using DLP lightcrafter with the lifecam cinema, i've installed everything following the TIDA and SDK guides, but i'm stuck in the calibration process because the white pattern is not shown, actually if i skip this step, the fine checker board doesn't appear either. i tried a solution propuse in the forum:
"In system_settings_projector.txt, change the value of LCR4500_SETTINGS_PATTERN_TRIGGER = 2 to LCR4500_SETTINGS_PATTERN_TRIGGER = 0"
i'm using lcr3000, i supossed my system_settings_projector.txt was config_projector.txt, and changed LCR3000_PARAMETERS_INPUT_TRIGGER_TYPE=2 to LCR3000_PARAMETERS_INPUT_TRIGGER_TYPE=0, this didn't work either, so i don't if i'm missing something, or the calibration does not work with lifecam
PS: actually, if i go ahead to 6 or 7 in the command line, nothing is projected by the lcr.
i hope you can help me.
best regards.
Sebastian.