This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dlpdlcr2000evm & UV for use in stereolithography

Other Parts Discussed in Thread: DLP2000

Hi all,

Not sure which is the right forum since this is a brand new part (please redirect if needed.) I noticed the new dlpdlcr2000evm which could be a great platform to experiment with SLA processes. Does anyone if it can be used with a UV light source instead of RGB LEDs?

Thanks!

  • Hi Jonathan,

    Thanks for your question and welcome to the DLP forums! The DLP2000 DMD is able to support wavelengths between 400 and 700nm so long as the thermal effects are considered. Please accept my friend request and we can take this discussion offline.

    Best,
    Paul