Other Parts Discussed in Thread: DLPLCR4500EVM,
Hi,
On one of our DLPLCR4500EVM boards, we have uploaded the firmware safely with "skip bootloader", but the firmware upload was aborted at around 10% and now we cant connect to it at all.
It seems that the reason for the failure is DEFAULT.AUTOSTART=1 option in the firmware, which instructs the DLP to boot into standby.
Now, I put J30 jumper in, to force the DLP into bootloader mode, but it goes into standby instead!
What options do we have to recover from this state?
1. We dont have a JTAG boundary scan cable to follow this guide: www.ti.com/.../dlpu017a.pdf
2. We have an ST-Link v2 JTAG programmer and it seems as J24 is a compatible connector to it. Could it work? Is there a guide?
3. What other options do we have to recover from this state?
Peter