Hello
What is the highest flux density damage threshold available for DMD chips, and which product has the highest damage threshold?
I am considering the possibility of using DMD's for a rather high-power application. It is in this context, that my question on damage threshold arises.
The light source could be either a broadband light source or a laser light source.
I need to do a spatial light modulation of about 3 kW of CW-power. Can this be done with only 1 DMD or should it be divided up onto several? In the latter case - how many DMD's would be needed?
Grateful for any advice you may be able to provide.
Regards, David