Part Number: DLPLCR6500EVM
Hello,
In the middle of using the DLP, the image projected on the DMD froze and was no longer being toggled to the image that was supposed to be projected next.
I was going to upload the most updated firmware on the DLP in order to reset the DLP and fix the frozen image issue however, the computer is no longer recognizing the DLP through the USB connection and on the GUI, it just says "Disconnected" and therefore, I am unable to upload the most up-to-date firmware.
We have been using the DLP consistently for over 8 months now and nothing has changed in the way the DLP is used (no additional watts of power provided, same settings, etc).
We're not sure what we should be doing next?
Thanks