Continuing my quest of writing a C program to communicate with the DLP I am now faced with a bunch of questions.
In regards to section 3.9 and 3.10 of the "dlpu007d.pdf" document (Programmers Guide):
1- How are the trigger delay bytes ordered, is byte 4 LSB or HSB?
2- How does one fill the trigger period bytes if not using auto-trigger mode?
3- How should exposure time bytes be filled in relation to trigger delay bytes, or in other words do these times accumulate or not?
4- How are exposure time bytes ordered?
5- As for byte 16, if I want a b&w sequence how do I fill it?
6- Pattern definition; should the data payload be filled as when uploading a static image but with the byte 0 of every packet's (that constitutes the bmp) payload w/ the number that represents the cardinality of that bmp in the sequence? Or should only the byte 0 of the first packet's payload have that cardinality with intermediate and last packets having just bmp data?
In regards to section 3.19 and 3.20 of the same document:
7- What is the purpose of the Load/Enable Custom Sequence ?
Thanks in advance