This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000: DLP9000

Part Number: DLP9000


What is the laser power at 2000 nm it can handle ? 

  • Hello Ashoke,

    I am sorry your question got missed.

    Welcome to the DLP section of the TI-E2E community.

    The DMD in question is not designed to work in this wavelength range.  The window has very poor transmission characteristics.

    Operation at this wavelength is outside the Recommended Operating Conditions in the data sheet and therefore would have no warranty.  

    Fizix.