This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC6401: Position Offset

Part Number: DLPC6401


Hi there,

I am able to communicate with the DLPC6401 using an Arduino UNO.

What I'd like to do is an offset of the displayed resolution.

In the datasheet, it seems to be associated to the Display Position in Frame register at address 0x66 (see the table below).

However, I'd like to move the displayed resolution on a specific (x,y) coordinate.

Is there a way to do so?

Kind regards,