There is a 4-pin connector J11 for I2C communication in DLP4710EVM-G2.
How to use this connector? What's the function of each of the 4 pins?
I read in a solved thread that there shouldn't be any hardware modifications needed to the board to get communication working with Arduino.
I tried to use the following Arduino code (learned from another solved thread) to turn the LED on but didn't succeed.
#include <Wire.h>
void setup()
{
Wire.begin();
Wire.beginTransmission(0x1B);
Wire.write(0x52);
Wire.write(0x02);
Wire.endTransmission();
}
void loop()
{
}
Is there anything else I need to do?
Many thanks in advance!
Eric