Part Number: DLP3000
Hi Ti,
Currently I am using the DLP3000 Light Crafter reference design and faced the below problem. Could you please help to advise?
1. I2C interface doesn’t support variable pattern sequence.
2. Does it support UART? They couldn’t locate any manual or commands regarding this.
3. On a dlpc350 for example, it only support up to 48bits. If the total projection is over the size of 48bits, how could it maintain the transfer rate? This is a broad question, might have several possibilities.
4. During projection, if the engineer alternate image from different 24bit it seems to have impact on producing a complete image on the projection side within the spec time.
5. The memory assignment is limited to it’s own memory arrangement. 7 bit for example must always start from another chunk of 8 bit memory.
6. DLP flashing firmware issue which failed in the mid of flashing.
7. Handling on flash connection failed.
8. When firmware too large, the flashing process failed probability is high. (10 MB)
9. If the image is a little bit complex, the probability of failing is high too. It might be related with Question 2 which due to the compression & decompression method it use.