This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: Reflectivity of DLPLCR4500EVM at 1064 nm

Part Number: DLPLCR4500EVM


Hello,

I would like to use the DLPLC4500EVM, which comes with the DLP 0.45 WXGA chipset and is officially rated for use with 400-700nm, to beam shape a variety of different laser wavelengths, some in the optical range and some in the near infrared particularly 1064 nm. Can you tell me what the reflectivity of this product would be around 1064 nm?

Thanks!

  • Joshua,

    Thanks for your interest in our DLP products.

    Some basic reflectivity information is listed in the DMD datasheet, but not at the wavelengths you describe. I'll investigate with my team and give you feedback by the end of the week.

    Best Regards,

    Philippe Dollo