Part Number: DLPLCR6500EVM
I shine a parallel light beam to the DMD screen vertical to the DMD screen and expect to get the two reflected light beams at both sides which should be at the same height with the light source. However, it seems that I have to rotate the DMD by around 30 degree to get the two reflected beams at the same level.
img1 and img2 are correspondent. img3 and img4 are correspondant. I want the two reflected beams at the same level without rotating the DMD. Do I need to set some parameters in the software?
img1 and img3 say how I shine a light onto DMD which is rotated by different angle. img2 and img4 are the reflected light beam projected onto the wall.
Hope you can help me. Thank you very much.
Yoolee.
img1 img2
img3 img4