This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP7000: Pattern Rate for DLP7000

Part Number: DLP7000

In the page of DLP high speed visible products, it says that the 8-bit pattern rate for DLP7000 could be up to 1900 Hz. While the specs of evaluation kits from Wintech and ViLUAX show that the max pattern rate for 8-bit is ~ 300 Hz, which is much slower than 1900 Hz.

So just wondering, any vendor provides DLP evaluation kit available for a high patter rate, i.e., 1000 Hz for 8-bit grayscale, or there is technical challenge for high patter rate?

Thanks a lot