Hi
I have a question about the DLP 7000 data sheet.
Although it is described as ”RArray-To-Ceramic = thermal resistance of DMD package from array to TC2 (°C/W)” in chapter 8.6.3,
Is the value of RArray-To-Ceramic as 9.0 [℃ / W] as described in chapter 7.5 Thermal Information?
If RArray-To-Ceramic = 9.0[℃ / W], I think that the value in chapter 8.6.3 is TP1 instead of TC2.
Best regards
Leonardo