Part Number: DLP3000
Hi TI Experts,
I have customer that would like to do a project on image projection.
> Is DLP3000 able to perform image projection on glass or windscreen?
> They would like to use an RGB laser module for the prototype as opposed to LED for lighting.
Is it possible to replace the LED to Laser module for DLP3000?
If not - do you have a component to recommend?
> Can they make any source code/firmware changes to the DMD?
> Can the DLP accept one image input at a time instead of steady stream of input video?
> What is the background that the DLP projected? Is it black light or transparent?
Thanks,
Br,
Teach Me