Other Parts Discussed in Thread: DLP4500NIR,
I am developing a board with DLPC350 to use a DLP4500NIR. According to DLPC350 datasheet, DMD interface traces should follow specifications of Table 19 (page 48). Table 21(page 49) provides the DLPC package output delay at the package ball. Total trace length includes packages skews, PCB length, and DMD flex cable length. How can I follow table 19 specifications instead some signal package skew is higher than recommendations. I don't know if I understand Table 21 values properly.