This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLIGHTCRAFTER: The more detailed geometric parameters for DLP LightCrafter

Part Number: DLPLIGHTCRAFTER

Hi,

I am a graduate student now working on a project using the DLP LightCrafter with laser. We took of the light engine so that we can utilize our custom laser and optical system, but after the disassembly the DMD mounting is not as firm as desired. We decide to make a metal module as the mounting similar to that of the light engine. It is a little bit difficult to get the best measurement of the current modules. I wonder if we could be provided with more detailed dimensions information or a CAD file for at least the light engine part of the LightCrafter. That would make it a lot easier for our development. Or you could send through email: wky2018@gatech.edu.

Thank you.

Kaiyue