This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: Ordering additional TIR prisms

Part Number: DLP4500
Other Parts Discussed in Thread: DLPC350,

Hi,

I wonder if it is possible to order additional TIR prisms that are used in the DLP4500 projector module.  We are developing applications using the DLPC350 + DLP4500 and would like to use the TIR prisms in the evaluation module.

Otherwise, are the specifications of the prism available such that we could get them manufactured elsewhere?

Many thanks!