Other Parts Discussed in Thread: DLPC350
Hello,
I have a few questions regarding the Lookup Table (LUT) in the EMV:
According to the EMV User Guide, there are limits when saving a solution on how many entries any given LUT can have at most
(max. 64 DEFAULT.SPLASHLUT [image index LUT] entries, max. 128 DEFAULT.SEQPATLUT [Pattern Definition] entries).
Is it possible to have more LUT entries (for example 300 entries in the SEQPATLUT) then the ones mentioned above?
And in the Programmers User Guide, what is the 'Number of patterns to display', and why can it range from 1 to 256?
Also, the GUI will let me add entries to the SEQPATLUT (Add Pattern to Sequence) even if it exceeds 128, but when trying to save the solution, it gives me the error message 'Error validating LUT data', but not when applying it. And the GUI stops working when trying to send the sequence.
Thank you.