Other Parts Discussed in Thread: DLPC2607
Hi,
I'm curious about the abilities of the DLP2000 to run at significantly higher framerates if a custom controller is used.
While the recommended display driver (DLPC2607) mentions an absolute maximum of 120Hz, the DLP2000 datasheet itself mentions no absolute framerate limit,
showing only a maximum clock of 80MHz, and describing the mirror switching speed as 'negligible' (DLP2000 datasheet, section 7.7.1).
Given that there are 12 data lines running at 80MHz DDR, it would seem to me the DMD itself should be capable framerates in the multiple kHz given an adequately fast controller and sufficient cooling.
Is the DLPC2607 the limiting factor here, or are there other limiting factors within the DLP2000 that keep it from running this quickly?