Hello! I am part of a robotics team at Carnegie Mellon University. We are looking at IR spectrometers for a project we’re working on. Ideally, we would like a spectrometer of <100g, so we are looking at the NIRscan nano device.
1. How much does the actual device weigh? Is it separate from the computer board? If so, how much does each component weigh? Can you use other computer boards instead of the one it comes with?
2. Temperature - what is the lowest and highest temperatures in which this device has operated/survived?
3. Can the device withstand a vacuum environment? Can it operate in a vacuum?
4. Sampling
- How close must we be to the sample (which will be on the ground)?
- Is there a recommended angle that works best?
- Is there a minimum strength of ambient sunlight needed?
5. Calibration - is the device calibrated specifically to work in Earth atmosphere? Would additional calibration be needed to operate in a vacuum?
6. What format is the data in? Size of data packet?
7. Are there any student or university discounts for this device?