Hi there
I'm currently having some problems with updating the splash screen images on our 3010-g2 device. I've tried using the DLP Lightcrafter v7.0 software, both the basic and advanced programs create the same behaviour.
Our custom splash screen images are being uploaded but its broken up and artefacty, I cannot change the input on the projector once this happens and it happens every time I try to use a custom splash screen. If I flash back to the normal firmware image all functionality is restored. I'm guessing the image formats I've tried are not supported but I've been at this all day and haven't got any closer. I've tried bitmaps, Jpeg (both CrCb 422 and 444) and also PNG files but all produce similar results, all files were made with GIMP 2. I've tried resolutions of 1280*720 and 640*360.
I've even used some of the images on our 3010 gen 1 device and it was working great. I'm not sure where to go from here.
Here is what I've been trying in the simple GUI;
Go to the firmware section, Click Update Flash Image "Get Started" button
select 3010-G2 from dropdown, select latest firmware downloaded from TI as source, name the output and click next
Skip looks
Add our splash screen to first splash location, click next
Apply a short axis flip as we are using rear projection, set default splash to 1, set LED currents, click finish
Then proceed with the update.
I've been trying similar with the advanced GUI and everything seems to work fine when I use the factory default splash screens, as soon as I try to include our own splash images the device becomes unusable with the broken image on screen and inability to change input.
Does anyone know of where I can get some sample images that I can inspect and compare with our splash images?
Or if anyone has any ideas what I'm doing wrong that would be great.
Thanks in advance
Steve