This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: A Status byte When DLPC350 is programming mode

Part Number: DLP4500

Hi

Let me talk about a Status byte using I2C for DLP4500.

I do not see a Status byte When it is programming mode

We try to read Manifacture ID(0x15,0x0C), We got these values.

[0]:0x83 // We gess it is not status byte, it seems Table A-4
[1]:0x14
[2]:0x08
[3]:0x48
[4]:0x00
[5]:0x00
[6]:0x20 // man id?
[7]:0x00 // man id?
[8]:0x00

I2C Read Transaction Sequence is described in Section 1.1.2 of Programmers guide

5. Host reads a status byte and checks that bit zero is set.


Should we not see the status byte When it is programming mode.

Best Regards
Hiroyasu