Hi I am looking for guidance and advice. I am looking for a pico/micro display that can be used to project the image onto a small piece of plastic. Plastic screen size approx. 40mm x 40mm. Can anyone help?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Philippe,
Thank you for your reply. I am looking to create a heads up display type set up. Do you think the EVM is sufficient to project onto a surface? Are the optics adjustable or is this something I would need to add?
Also is the EVM Plug and play? So I can test the idea?
Help much appreciated.
Daniel