This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/DLP4500: dlp4500

Part Number: DLP4500

Tool/software: TI C/C++ Compiler

Hello ,

Please anyone suggest me solution my problem.

I am working on DLP4500, i would like to know what parameters in the config folder would influence the system calibration. I have created a calibration board for A3 format and i tried to calibrate my camera calibrations works out fine with re-projection error 0.2 but in system calibration (Projector calibration] the re-projection error is  going beyond 5 and some times to 30.

.I have created a calibration board  7x10 with row and column distance as 10mm. Is it mandatory to use the same calibration image that is provided in side the folder

calibration/camera _images?

How can i solve this issue?

With Regards

Ramyampet Vinaykumar  

  • Hello Ramyampet,

    You can generate a different calibration image by running the program and then calibrate with that image. And every setting in that folder will have an impact on calibration to some degree. It will require consideration of the entire system and environment for proper optimization.

    Thanks,
    Kyle