In an earlier post from this forum: https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/video_and_data_display/f/947/t/520399?tisearch=e2e-sitesearch&keymatch=240hz
It mentioned that the frame rate of an old DLPC is due to the 150MHz so 60Hz with 1920*1080.
It further mentioned that in order to achieve higher frame rate with that controller, the reduction of input resolution would help.
So with the current DLPC4422 300MHz and working 120Hz with 4k. Is it possible to lower the resolution to 1920*1080 to achieve 240Hz?
I am desperate in finding a solution to make a DLP 240Hz projector with 720p or 1080i and full color (not 8bit for sure)