Other Parts Discussed in Thread: DLP2000
Hi,
I want to display the RGB out of renasas controller to DLP2000 projector. As per the pinout i connected hsync, vsync, dataenable. pclk and rgb pins to the host pins. but nothing happens.(just red color screen)
In the user guide. It is not properly explained about, how to interface this dlp2000 evm with an external host processor other than beaglebone.
Actually I don't know what to do with these pins HOST_PRESENTZ, VINTF, PROJ_EXT_ON.
Do I need to connect I2c pins for Displaying the RGB output to the projector.
Is this DLP2000 EVM works when I connected these RGB pins alone to external processor.
I need proper explanation for all these questions
1. what all pins are connected to RGB pins?
2. what about the pin assignment of PDATA pins to RGB pins of Host processor?
3. What should do with these PROJ_ON_EX, HOST_PRESENTZ, J3 header etc?
Can anyone please help me...
Thanks in Advance