This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: Loading pattern from matlab automatically

Part Number: DLP4500

Hi all,

Is there a method that could load the patterns from matlab automatically after gettering patterns by matlab, rather than adding pattern one by one, build firmware, and upload firmware manually? It takes a lot of time to build firmware manually.

I use the DLP GUI to control the DLP, version: DLP LightCrafter 4500 Control Software v3.1.0.

Thanks,

Mei